View all news

Arrow Electronics Extends Global Secure Provisioning Services for IoT Devices

02/25/2019
Cypress, Infineon, Microchip Hardware-based Security Devices and NXP Semiconductors Secure Elements and Microcontrollers are Supported Globally

NEU-ISENBURG, Germany-- Arrow Electronics has extended its global secure provisioning service to cover silicon from Cypress, Infineon and Microchip in addition to NXP Semiconductors Secure Elements, which participated in Arrow’s initial offering launched in 2018. The service enables the rapid deployment of IoT edge nodes and gateways featuring hardware-based security features. Secure provisioning capabilities will be made available to Arrow’s customers globally.

Aiden Mitchell, vice president IoT, Arrow Electronics said, “Cybersecurity is a high priority for developers, particularly with requirements such as the European GDPR legislation and the responsibility it places on organisations to protect data and security. This means that the ability to authenticate IoT devices and quickly establish trusted connections to the cloud is now an essential element of any product deployment.”

Arrow’s programming and provisioning technology is based on a highly secured and reliable chain of trust. This consists of relationships with leading global domain experts on device security and Certificate Authorities; the secured transfer of customer IP and security credentials; and highly secure programming platforms. There is support for registration for device certificates at multiple cloud service providers, and certificate lifecycle management services are also available.

Arrow offers complete end-to-end security solutions, including cybersecurity. These secured provisioning services are just one building block out of Arrow’s comprehensive portfolio of technology from sensors, wireless connectivity, gateways to cloud platforms, data ingestion, aggregation and visualization, analytics and security. Service capabilities span ideation, design, integration, manufacturing, logistics, financing, wireless connectivity with billing services, marketing, monitoring and managed services, and sustainable and secured end-of-lifecycle disposition. The latter is becoming ever more significant with the onset of privacy legislation.

Arrow will present its secure provisioning services at Embedded World trade show in Nuremberg, Germany (Stand 4A-340, February 26-28). For more information customers can reach out to: secure.provisioning@arrow.com

Appendix

The following technologies are currently supported by Arrow Electronics’ secure provisioning services:

Cypress PSoC® 64 Secure MCUs
The new Arm® PSA-Certified PSoC 64 Secure MCUs integrate robust, standards-based system layer security software with the hardware layer features available in the ultra-low-power PSoC 6 architecture. Specifically, PSoC 64 Secure MCU devices provide an isolated root-of-trust with true attestation and provisioning services. In addition, the line includes devices that deliver a pre-configured secure execution environment supporting the system software of various IoT platforms, providing TLS authentication, secure storage, and secure firmware management. The MCUs also include a rich execution environment for application development, with an RTOS that manages communications with the secure execution environment. Arrow has been selected as a preferred provisioning partner by Cypress.

Infineon OPTIGA™ Trust X
With the increase of connected devices and applications, the need for strong device authentication with the cloud and secured communication protocol is significant. Infineon offers the OPTIGA Trust X as a turnkey security solution for industrial automation systems, smart buildings and smart homes as well as consumer devices. The security controller comes with full system integration support for easy and cost-effective deployment of high-end security for IoT devices. Arrow is a preferred partner of Infineon`s Security Partner Network (ISPN) and offers fully customized provisioning of keys and credentials.

Microchip SAML11 MCU
Microchip’s new SAM L11 MCU is based on the Arm® Cortex-M23 core, with the
SAM L11 featuring Arm® TrustZone® for Arm®v8-M, a programmable environment that provides hardware isolation between certified libraries, IP and application code. Arrow has been selected as a provisioning partner for this product by Microchip.

NXP A71CH Secure Element and security enabled MCUs
NXP’s broad portfolio of scalable security solutions includes secure elements and microcontrollers. The NXP A71CH Plug & Trust is a ready-to-use security solution that has been developed to secure IoT peer-to-peer or cloud connections in smart home/city and industrial applications including sensor networks and IP cameras. The solution is based on a root of trust at the silicon level with security functions including encrypted key storage, key generation and derivation to protect private information and credentials for mutual authentication. The A71CH can be provisioned by Arrow with the credentials necessary for autonomous cloud onboarding and peer-to-peer authentication. Arrow expands the secure provisioning of NXP devices to uniquely include NXP’s next generations of secure elements as well as security-enabled microcontrollers.
 

 

Multimedia Files:

View all news